Skip to main content
Please Select Your Country/Language Preferences

Case Studies

industrial plant
Bus Systems
Case Studies
See how our Infrastructure Solutions solve our customer’s challenges.
Swift Action and Expertise

Bus Duct Emergency Response: Swift Action and Expertise

Our team gets company's power generation system back online and fully operational within two weeks of a catastrophic lightning strike.

Learn More
Rapid Response to Transformer Explosion at Power Plant

Rapid Response to Transformer Explosion at Power Plant

We've designed, built, shipped, installed, and commissioned replacement SF6 gas insulated line (GIL) in just 39 days.

Learn More
GAS INSULATED LINES GIL APPLICATION-

SF6 Gas Insulated Lines (GIL) application guide

One of the challenges in the design of a power plant substation is how to maximize its potential while maintaining safe conditions for workers and the surrounding environment.

Learn More
Bus Systems Retrofit

Retrofit GIS Install in Older Bus System

Substations often require new equipment to upgrade or expand existing facilities or replace damaged systems. This often requires interfacing to equipment from varying manufactures and technologies of existing equipment.

Learn More
Bus Systems Future Expansion

Future GIS Bus System Expansion

Many of the same challenges presented by a retrofit project are also encountered when expanding existing stations. There are various interfaces to be designed and restrictive outages schedules that must be adhered to.

Learn More
Bus Systems Tunnel and Vertical Shafts

High Voltage Bus Vertical Installation

Hydroelectric generating stations often require transmission of power over large vertical distances. Transmitting power at transmission voltages rather than generation voltage, is more economical.

Learn More
Bus Systems Elevated

High Voltage Bus Elevated Installation

Every station layout design has certain physical boundaries to which the transmission components must adhere. If the space available precludes the use of air-insulated bus and a lack of available land prevents continuous transmission line at ground level or below grade, a high voltage bus elevated installation provides a potential solution.

Learn More
Bus Systems Below Grade Transmission

High Voltage Bus Underground Installation

Below grade transmission installations offer the advantage of lower installation costs in open areas. Trenches can be used when crossing roads or installing in areas where water tables are close to ground level.

Learn More