Skip to main content
Please Select Your Country/Language Preferences

Retrofit GIS Install in Older Bus System

industrial plant
CASE STUDIES
Retrofit GIS Install in Older Bus System

Substations often require new equipment to upgrade or expand existing facilities or replace damaged systems. This often requires interfacing to equipment from varying manufacturers and technologies of existing equipment.
 

Bus Systems Retrofit Older GIS Installs

In the case of a retrofit GIS install to an existing gas insulated switchgear substation, the ability to design and install a variety of interfaces, and to allow sufficient installation tolerance is paramount. The existing equipment may include GIS supplied by different manufacturers who may adhere to contrasting philosophies and operating parameters.

In other retrofit cases, outdated equipment must be replaced. Again, the challenge remains to minimize the outage time required to implement the change and to utilize as much existing peripheral equipment at possible to reduce costs. Our High Voltage Bus Systems provides solutions to the problems faced when retrofitting or extending existing systems and offers turnkey installations and commissioning.

Retrofit GIS Install Project Profile: Consolidated Edison Dunwoodie Station (Yonkers, New York)

The Dunwoodie substation, commissioned in 1974, functioned well until 1988, when an oil cable fire destroyed a circuit breaker, the adjacent oil pot heads, interconnecting breaker bus and disconnects.

In rapid response to Consolidated Edison’s emergency requirements, we have provided interconnecting breaker bus to bypass the damaged breaker position and re-energize the ring. The bus left future expansion capabilities to interface to a new circuit breaker position that would be supplied at a later date. The interconnecting bus required interface to existing ITE bus. High Voltage Bus Systems was the only manufacturer that could respond to this emergency.

Seabrook Nuclear Power Plant Substation (Seabrook, New Hampshire)

The Seabrook gas insulated substation project, consisting of 345 kV ITE GIS and bus, had developed a history of unreliability due to leaks and insulator failures within the bus. This was particularly a cause of concern within areas of the substation that were not protected by redundant sections of the installation, thereby having no backup in case of section bus failures.

Our bus system, backed by its established record of reliability in long-term service, was selected to replace the ITE bus for these critical connections. The retrofit gis install involved connections from the GIS to both main transformers and to auxiliary transformers.

In addition to offering a reliable bus design, High Voltage Bus Systems defined and managed a schedule to complete the installation within a one-week outage to comply with the NRC approved outage schedule, and under tight space and access conditions.

The first of the Seabrook bus installations has been in service without fault since its completion in 1990.

To learn more about our offerings, visit Bus Systems and Bus Services

CONTACT US


Request More Information 

To receive a quote or request additional information, use the button below to access the appropriate contact form. 
Request More Information

Bus Duct Emergency Response: Swift Action and Expertise

Our team gets company's power generation system back online and fully operational within two weeks of a catastrophic lightning strike.