Aerospace and Defense Overview
Proven Rugged Electronics Packaging - For the Past 50 Years
Systems are becoming smaller and more powerful, thereby driving the need for enhanced thermal dissipation. nVent SCHROFF offers solutions to satisfy these SWaP (size, weight and power) trends for critical systems such as ATR’s, data recorders, mission computing systems, surveillance or payload management systems.
You can count on nVent SCHROFF for complete mechanical, electronic, and thermal solutions supported by a team of experienced engineers and test laboratories. We understand now more than ever the importance of component failure being a non-option.
From EMC and Seismic Cabinets to rugged subracks, capable of withstanding up to 60kg or 25G of shock, to SWaP friendly solutions to retain and cool printed circuit boards - we have you covered.
Solutions for a Wide Range of Applications
Explore the interactive hotspots below to see application-specific products, resources, and more.
Quality you can count on
We can provide the certification and procured part tracing you may need for government programs. Learn more about the quality certifications that we maintain to connect and protect your equipment when this mission is critical.
- AS9100 and ISO9001:2015 Certified
nVent SCHROFF's San Diego, California location has been AS9100 Rev D standard since 2017. Per the International Aerospace Quality Group (IAQG), all aerospace suppliers shall be certified in order to meet the stringent quality requirements of the industry.
- Calibration Program - ISO 17025:2005
Our Calibration Program follows general requirements for the competence of testing and calibration laboratories as set by ISO 1025:2005
- Counterfeit Parts Prevention Program
We have a robust Counterfeit Parts Prevention Program in place to ensure all purchases of commpdities and electronic components used in enclosures and components for enclosures are sourced only through OEMs or authorized distributors
- First Article Inspection - AS9102
We maintain a strict adherence to FIA to ensure that our engineering, design, and specification requirements are properly followed
- International Traffic in Arms Regulation (ITAR)
nVent SCHROFF has been servicing U.S. based customers for over 50 years and we are committed to maintaining ITAR discretion for our customer base. We regularly train employees in the ITAR procedures, provisions, and compliance to handle sensitive information. We also maintain separate systems only available to authorized U.S. personnel.
- Foreign Object Debris (FOD) Prevention
We use the FOD quality control concept to drive an internal program that maintains our high quality of product and safety for our staff
- Life Cycle Management
Component transition, obsolescence, and end of life (EOL) are inevitable. nVent SCHROFF is committed to minimizing these disruptions and providing our customers with a seamless transition to keep vital operations running and protect your investment
- Space Qualified Manufacturer
Our retainers are designed for upper atmosphere and outer space applications using non-outgassing components and ink
- JOSCAR Registered Supplier
JOSCAR (the Joint Supply Chain Accreditation Register) is a collaborative tool used by the aerospace, defence and security industry to act as a single repository for pre-qualification and compliance information. Using JOSCAR can determine if a supplier is “fit for business”.
Our San Diego facility is the center of excellence for board retention and cooling. We're well known for our Calmark and Birtcher products that are all made in this facility, but also manufacture milled enclosures and conduction cooled assemblies, here as well. We are constantly innovating to keep up with increasing SWaP requirements and are committed to making sure we meet those requirements while maintaining the highest quality standards possible. The San Diego team is committed to driving the innovations and quality standards Schroff is known in board retention and cooling including:
- ITAR compliant and AS9100 certified facility
- Lot traceability from milling to final assembly
- Inspection at every step: IM and CMM, Final Inspection, FAI
- DFARS compliant
- Flow Downs for Chem/Phys Certifications
- Constantly innovating to keep up with increasing SWaP requirements with high-performance designs
- Made in America with Advanced Quality Systems meeting aerospace standards

Products and Services
Electronics protection tailored for your application
Humble or harsh environment, nVent SCHROFF solutions safeguard vital electronics. From PCB retention and cooling, to rugged subracks and seismic cabinet, to full VPX embedded chassis, you can rely on nVent SCHROFF to keep your systems up and running.
High Performance Products:
- Components for PCB retention, extraction and cooling
- VME64x, cPCI, VPX backplanes
- Conduction cooled assemblies
- Rugged milled enclosures
- 19" front panels, MIL COTS rugged subracks and cabinets
And the technical expertise to put them together to create solutions and overcome challenges.
From Components to Full Solutions - And Everything in Between
Our engineering team members are experts in innovative ways to get more heat out of your boards. We offer:
- Comprehensive consultation from the very beginning.
- Ability to work with existing board, frame, or chassis designs
- CAD templates and 3D printed prototypes available
- Thermal design, simulation and analysis services
- Over 60 years of experience as an industry leader in board retention and cooling
Take a peek at our Conduction Cooled Assembly video to learn more about what the journey from start to finish looks like for our customers.

Resources
Supporting the Best in the Business
nVent SCHROFF supports the leading government agencies and systems integrators for successful deployment of MIL-SPEC systems and COTS electronics in harsh environments.

Tier 1 MIL/AERO Customer
I wanted to drop you a quick note of super appreciation to your company, but specifically for the world class support from your customer service team. It had been our misstep in requesting this PO late and we had a customer in a line down position.
Your team was super responsive, clear and direct with all communications. We were provided all the details, including a strong milestone, as well as regular emails and updates which provided strong improvement each time.
Again, my sincere appreciation and gratitude to have a partner like Schroff who can step up in tough times, and even more happy to have a contacts within your customer service team who provide such great added value which they make seem effortless.
– Director, Sales & Global Business Development
Tier 1 MIL/AERO Customer
Wow, you all just made our day!!! Appreciate the team jumping on this one so quickly.
Mistakes will happen – it takes a great team to make them right!
– Sr. Specialist, Procurement
Tier 1 MIL/AERO Customer
In my experience, it has been rare to have someone who is both knowledgeable and extremely courteous in supplier Quality Compliance groups. I am very favorably impressed with my interactions with nVent SCHROFF.
– Principal Quality Engineer