Engineered Solutions that Protect Against EMP Threats
What is an Electromagnetic Pulse (EMP)?
EMP stands for Electromagnetic Pulse, which is a burst of electromagnetic radiation that can be caused by natural or man-made events. EMPs can cause damage to electronic devices, power grids, and communication networks, which can have significant impacts on society.
A natural EMP can be caused by solar storms or other high-energy events in space, while a man-made EMP can be created by nuclear detonations, high-altitude nuclear explosions, or intentionally designed EMP weapons.
When an EMP occurs, it generates a strong electromagnetic field that can induce electrical currents and voltages in conductive materials such as wires, antennas, and electronic devices. These induced currents and voltages can cause damage to electronic components, power grids, and communication networks, leading to disruptions in critical infrastructure and services.
To mitigate the potential impacts of an EMP, various measures can be taken, such as shielding critical electronics and infrastructure, hardening communication networks, and implementing backup power and communication systems.
How is an EMP diffused?
Diffusing an EMP depends on the source of the pulse and the strength of the electromagnetic field. There are several ways to diffuse or mitigate the effects of an EMP:
- Shielding: Shielding is one of the most effective ways to protect electronic devices from the effects of an EMP. Shielding can be accomplished by using conductive materials, such as copper or aluminum, to create a Faraday cage or shield around sensitive electronics.
 - Hardening: Hardening involves designing electronic devices and systems to withstand the effects of an EMP. This can be done by using specialized components and materials that are less susceptible to electromagnetic interference.
 - Grounding: Grounding is an important technique to protect against an EMP. By grounding electronic devices and equipment, any induced currents or voltages can be safely diverted away from the equipment and into the ground.
 - Redundancy: Another way to diffuse the effects of an EMP is to have redundant systems in place. This includes backup power sources, communication networks, and equipment that can be quickly deployed in the event of an EMP.
 - Preparedness: Finally, preparedness is key to mitigating the effects of an EMP. This includes conducting risk assessments, developing emergency response plans, and training personnel to respond to an EMP event.
 
Overall, the best way to diffuse an EMP is through a combination of these techniques, tailored to the specific needs and requirements of the electronic systems and infrastructure in question.
With EMP hardened technology, nVent TRACHTE has you covered.
Choose from additional security customization options to better protect critical equipment and personnel from safety threats. nVent TRACHTE buildings with EMP hardened technology are designed to securely shield systems, instrumentation, and personnel from the impacts of electromagnetic pulses. We apply patented EMP mitigation techniques and engineered EMP-resistant materials to all points of entry and building penetrations including entry doors, HVAC openings, cable tray, and conductors. nVent TRACHTE EMP-resistant buildings are factory and site tested in accordance with the Electric Power Research Institute (EPRI) EMP testing methods. Learn more about EMP solutions from nVent TRACHTE here.