Skip to main content

PYROTENAX Blog

[sivusto:tuotemerkki] Uutiset

1-10 of 10
fire ratd wiring in tunnels and construction.jpeg

When Does 2” Not Equal 2 Hours?

Many buildings use concrete construction methods as a way to protect wiring to critical circuits. This process of encasing standard building wires supplying power to critical life-saving equipment with up
sustainability and electrification_00 general (3).jpg image

Wiring A More Sustainable and Electrified World

- PYROTENAX System 1850 mineral insulated (MI) power wiring systems make it possible. In the quest to build a more sustainable and electrified world one of the fundamental requirements is
AdobeStock_205591838

Case Study: Urban Commercial Building Retrofit – Electrification Upgrade

When a retrofit project came up requiring the installation of a fire-rated solution that could also deliver a significant increase in ampacity without consuming extra space, it was no surprise
San Francisco Skyline with Dramatic Clouds at Sunrise, California, USA

Why PYROTENAX System 1850 MI Cable?

When it comes to the protection of critical electrical systems in buildings, there are a few different options to meet industry codes and standards. One of those options is UL2196
AdobeStock_112722445.jpeg image

Protecting Critical Building Circuits From Fire – Codes, Standards And Why Splices and Systems Matter

Fire safety and electrical codes and standards have been adopted worldwide and have been continuously improved to help ensure the best methods and practices for designing buildings. Important Area in
Hospital

Why Type MI is Specifically UL2196 Approved Fire-Rated Cable For Use in Hospitals

While designing commercial buildings, such as healthcare facilities, it is easy to overlook critical aspects of code. What is unique about healthcare facilities is the need to ensure that occupants
Big fire in the building

Beyond UL 2196 – Important Safety Findings for Fire Rated Cable Systems

If your building contains a fire rated wiring system providing power to critical life safety applications (fire pumps, emergency lighting and smoke evacuation, etc.), the standard you need to follow
pyro for healthcare

Why Fire-Rating Wiring is Crucial in Healthcare Buildings

When an emergency happens in a medical building, the need for quick response and protection of critical circuits is dire. In fact, medical professionals have a protocol to quickly respond
Construction work site

What is a UL Two Hour Fire Rating?

When it comes to fire rated wiring, there is a lot of discussion around safety standards and codes that building professionals need to follow. Let’s discover who is behind these
fire chiefs approve pyrotenax.jpg

3 Reasons Fire Chiefs Endorse 2 Hour Fire-Rated Cable

For Fire Chiefs, safety is paramount in an emergency situation. In fact, Fire Chiefs rely on a series on NPFA codes to provide essential benchmarks for a safe response to