Service Request for Cooling Units
Step 1. Troubleshooting guide to find a solution for your issue:
1. Excessive formation of condensate
- Cabinet with degree of protection less than IP54
 a. Check that the self-adhesive rubber seal between the air conditioner and the cabinet has been applied properly
b. Check that the closing panels of the condenser have been properly assembled
c. Check that there are no openings in the cabinet
2. Does not cool adequately
- Internal fan runs, compressor and external fan operate intermittently
 a. Clean the evaporator
b. Make sure that there are no external causes which limit the flow of air inside circuit
- Condenser fan and evaporator fan operate and compressor operates intermittently
 a. High pressure switch intervention, when present
Ambient temperature higher than the maximum allowed by the rating plate
- Ventilate the room
 
Please fill in the detailed error description and send the form
- Dirty filter
 
Clean or if necessary replace the dirty filter
- Dirty exchange condenser
 
Clean the condenser
- Ventilation short-circuiting
 
Make sure that no obstructions or obstacles may cause exhaust air short-circuiting
Check that the minimum distances from a wall, ceiling, electrical cabinet or another air conditioner is respected as indicated in this manual
b. Compressor thermal protector intervention
Air temperature in the cabinet higher than the maximum value allowed by the rating plate of the unit
Same causes and remedies reported at 2.a
- Internal fan operates, external fan does not operate, compressor operates intermittently
 a. Faulty fan electric condenser
- Replace the electric condenser
 
b. Faulty external fan
- Replace the condenser fan
 
3. Does not cool
- None of the components operate
 a. No voltage to the unit
- Make sure doors and switches are closed
 
- Compressor, condenser fan and evaporator fan operate
 a. Insufficient gas charge in the cooling system
- Please fill in the detailed error description and send the form
 
b. Compressor mechanical fault
- Please fill in the detailed error description and send the form
 
- External fan and internal fan operate, compressor does not operate
 a. Faulty fan electric condenser
- Replace the electric condenser fan
 
b. Faulty evaporator fan
- Replace the fan
 
- External fan, internal fan and compressor operate
 a. Adjusting thermostat faulty or set at a temperature higher than the temperature in the cabinet
4. ALARM
- ALARM
 P1, P4, HA, LA, HP, SEC, HAS,
Please fill in the detailed error description and send the form.
Step 2. Service Request for Cooling Units
If the issue with your air conditioner persists after trying the troubleshooting steps, please complete the form below. Have your Air conditioner details at hand, as you will need to provide them to submit the form. Refer to the image below for your product information.